Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description

RMC Wizard Window (Basic LTE-A Pro FDD Uplink)

To set up a UL reference measured channel (RMC), for a Basic LTE-A Pro FDD Uplink carrier, click the Wizard button in the Uplink node to open the UL RMC Wizard.

UL RMC Configuration (UE Test based on 36.521-1)

System Bandwidth 

Choice: 1.4MHz(6RB) | 3MHz(15RB) | 5MHz(25RB) | 10MHz(50RB) | 15MHz(75RB) | 20MHz(100RB)

Default: 5MHz(25RB)

Double-click or use the drop-down menu to set the system bandwidth (= Channel Bandwidth) and number of resource blocks for the reference measurement channel.

For more details, refer to 3GPP TS 36.521-1.

Modulation 

Choice: QPSK | 16QAM

Default: QPSK

Double-click or use the drop-down menu to set the modulation for the reference measurement channel.

For more details, refer to 3GPP TS 36.521-1.

Allocated resource blocks

Double-click or use the drop-down menu to set the allocated resource blocks for the reference measurement channel.

Couplings: Choice parameters coupled to the System Bandwidth and Modulation parameters.

For more details, refer to 3GPP TS 36.521-1.

RB Position

Choice: Lower End | Upper End

Default: Lower End

Double-click or use the drop-down menu to set the resource block (RB) position for the reference measurement channel.

Lower End: PUSCH RBs are inserted into the lower frequency end of the system bandwidth.

Upper End: PUSCH RBs are inserted into the upper frequency end of the system bandwidth.

For more details, refer to 3GPP TS 36.521-1.

Reference Channel for nMHz QPSK with full or partial RB allocation (nRB)

Channel Bandwidth

Displays the channel bandwidth of UL reference measurement channel based on the RMC configurations. This is a read only parameter.

For more details, refer to 3GPP TS 36.521-1.

Allocated resource blocks

Display the allocated resource blocks of UL reference measurement channel based on above RMC configurations. This is a read only parameter.

For more details, refer to 3GPP TS 36.521-1.

DFT-OFDM Symbols per subframe

Displays the DFT-OFDM symbols per sub-frame of UL reference measurement channel based on above RMC configurations. This is a read only parameter.

For more details, refer to 3GPP TS 36.521-1.

Modulation

Displays the modulation of UL reference measurement channel based on above RMC configurations. This is a read only parameter.

For more details, refer to 3GPP TS 36.521-1.

Target Code rate

This parameter is not applicable for the Basic carrier. Basic carrier does not support transport channel coding.

If you want to set exact same setting according with 3GPP standard, use the Advanced carrier.

For more details, refer to 3GPP TS 36.521-1.

Payload size (bits)

This parameter is not applicable for the Basic carrier. Basic carrier does not support transport channel coding.

If you want to set exact same setting according with 3GPP standard, use Advanced carrier.

For more details, refer to 3GPP TS 36.521-1.

Transport block CRC (bits)

This parameter is not applicable for the Basic carrier. Basic carrier does not support transport channel coding.

If you want to set exact same setting according with 3GPP standard, use Advanced carrier.

For more details, refer to 3GPP TS 36.521-1.

Number of code blocks per Sub-Frame

This parameter is not applicable for the Basic carrier. Basic carrier does not support transport channel coding.

If you want to set exact same setting according with 3GPP standard, use Advanced carrier.

For more details, refer to 3GPP TS 36.521-1.

Total number of bits per Sub-Frame (Bits)

Display the total number of bits per sub-frame of UL reference measurement channel based on above RMC configurations. This is a read only parameter.

For more details, refer to 3GPP TS 36.521-1.

Total number of symbols per sub-frame

Display the total symbols per sub-frame of UL reference measurement channel based on above RMC configurations. This is a read only parameter.

For more details, refer to 3GPP TS 36.521-1.

UE Category

Display the UE category of UL reference measurement channel based on the above RMC configurations. This is a read only parameter.

For more details, refer to 3GPP TS 36.521-1.